About "i.MX6 DDR Stress tester"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About "i.MX6 DDR Stress tester"

Jump to solution
1,461 Views
okamotosatoshi
Contributor IV

Hello.

I want to check about i.MX6Q.

I want to enforce the "i.MX6 DDR Stress tester".

Please let me check the following.

①Could you the latest version of the "i.MX6 DDR Stress tester"?

 I own the "DDR_Stress_Tester_V1.0.2".

②There is a specification of 1.2GHz (i.MX6Q) in "3.Select the ARM core speed" of User_Guide.

 It is a "MCIMX6Q5EYM10AC" of the devices used.

 This device is Frequency (1GHz).

 Even in this case , ARM core speed will be set at 1.2GHz?

Regards,

-okamoto

Labels (1)
Tags (3)
1 Solution
1,171 Views
Yuri
NXP Employee
NXP Employee

Strictly speaking, to be fully on safe side, it is NOT correct to configure MCIMX6Q5EYM10AC for 1.2 MHz. 

View solution in original post

0 Kudos
Reply
4 Replies
1,171 Views
okamotosatoshi
Contributor IV

Hi, Yuri

Thank you for reply.

Quad and DualLile was mistaken set the 1.2GHz.

"MCIMX6Q5EYM10AC" will is set 1.0GHz.

Regards,

-okamoto

0 Kudos
Reply
1,171 Views
Yuri
NXP Employee
NXP Employee

1.

Basically it is quite enough to use the "DDR_Stress_Tester_V1.0.2".

i.MX6 DDR Stress Test Tool V1.0.2

2.

"MCIMX6Q5EYM10AC" is not qualified for 1.2 MHz. This means, that customers

can try the device under 1.2 MHz, but we cannot guarantee proper operations with

parameters, provided in the Datasheet(s). Device lifetime also may be affected,

when using the device under non-specified conditions.    


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,171 Views
okamotosatoshi
Contributor IV

Hi, Yuri

Thank you for reply.

I have fixed the Version.

Is it correct to be set on either the frequency?

(This deveice("MCIMX6Q5EYM10AC") 1GHz or 1.2GHz.)

Regards,

-okamoto

0 Kudos
Reply
1,172 Views
Yuri
NXP Employee
NXP Employee

Strictly speaking, to be fully on safe side, it is NOT correct to configure MCIMX6Q5EYM10AC for 1.2 MHz. 

0 Kudos
Reply