About power supply voltage setting in Linux BSP L3 .0.35 for MX6DL-SABRE-SDP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About power supply voltage setting in Linux BSP L3 .0.35 for MX6DL-SABRE-SDP

776 Views
yuuki
Senior Contributor II

Dear all,

We use Linux BSP L3.0.35(LTIB).

However, we have the problem that a system reboots in the middle of Boot.
We want to check a set point of each power supply voltage in U-Boot

- VDDARM_CAP
- VDDSoC_CAP
- VDDPU_CAP
- VDDARM_IN
- VDDSOC_IN


Would you tell me the point that we should confirm?

File position / File name / Checkpoint

It is necessary for us to check it as soon as possible.

May I have advice?

Best Regards,
Yuuki

Labels (2)
0 Kudos
Reply
1 Reply

628 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

please check attached Linux Manual Chapter 18
Low-level Power Management (PM) Driver, Chapter 19,20,21

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply