About latch timing of EIM read operation in i.MX6DQ.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About latch timing of EIM read operation in i.MX6DQ.

Jump to solution
556 Views
keitanagashima
Senior Contributor I

Hi All,

Which is right latch timing EIM_BCLK or EIM_FB_BCLK?

I think that rising edge of EIM_BCLK is correct latch timing.

And, EIM_FB_BCLK looks using for skew adjustment like a below DLL. 

Is my understanding right?

埋め込み画像 2

 

Best Regards,

Keita

Labels (3)
0 Kudos
Reply
1 Solution
464 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Yes, rising edge of EIM_BCLK is correct latch timing.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
465 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Yes, rising edge of EIM_BCLK is correct latch timing.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply