About i.MX6Solo DDR3 sdclk wiring lengs.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About i.MX6Solo DDR3 sdclk wiring lengs.

ソリューションへジャンプ
906件の閲覧回数
takashitakahash
Contributor III

Dear community.

Our customer has question below.

The wiring length of DRAM_SDCLK [1: 0] is described as max 2.25 inch,
When DDR 3 branches into two, the wiring length becomes A + C in the case of DDR 3 _a, A + B in the case of DDR _ b,
Do I have to meet  A + C <2.25 inch and A + B <2.25 inch respectively?

Or will it be 2.25 inches including the other branches? (A + B + C <2.25 inch)?

pastedImage_1.png

pastedImage_2.png

ラベル(1)
0 件の賞賛
返信
1 解決策
824件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

it is necessary to meet  A + C <2.25 inch and A + B <2.25 inch respectively.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
825件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

it is necessary to meet  A + C <2.25 inch and A + B <2.25 inch respectively.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信