Dear All,
Hello. I have a question about internal boot ROM processing in i.MX6SDL.
Refer to the below device status register in eMMC card.
The "DEVICE_IS_LOCKED" bit had changed to "1" in eMMC card on my customer's board.
(eMMC Status : 1 = Device locked)
And, the board couldn't boot-up (No output to serial console).
[Question]
Does iROM in i.MX6SDL check this bit 25 and does stop access to eMMC?
Could you check the internal ROM code?
Best Regards,
Keita
解決済! 解決策の投稿を見る。
HI Keita
ROM does not check/change this bit. eMMC itself check it and
if locked, do not provide data to host. This is described in
sect.7.6.13 Card lock/unlock operation eMMC 4.41 specification
JESD84-A441.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
HI Keita
ROM does not check/change this bit. eMMC itself check it and
if locked, do not provide data to host. This is described in
sect.7.6.13 Card lock/unlock operation eMMC 4.41 specification
JESD84-A441.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear Igor,
Hello. Thank you very much!
Best Regards,
Keita