About changing the VPU clock in i.MX6DQ.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About changing the VPU clock in i.MX6DQ.

跳至解决方案
895 次查看
keitanagashima
Senior Contributor I

Dear All,

Is it possible to change the VPU Clock source from PLL2_PFD2 to PLL2_PFD0?

My customer doesn't use the PLL2_PFD0 for any other.

Is there some impact?

Device i.MX 6Dual

BSP: jb4.2.2_1.1.0 (L3.0.35)

Best Regards,

Keita

标签 (4)
0 项奖励
回复
1 解答
599 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

Fushi PengEmployee

105675_105675.pngpastedImage_0.png

usually PLL2_PFD0 is used by LVDS. LVDS clock is not expected to be changed. If there is no any other module which used PLL2_PFD0, VPU clock can be configured to use PLL2_PFD0.

在原帖中查看解决方案

0 项奖励
回复
1 回复
600 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

Fushi PengEmployee

105675_105675.pngpastedImage_0.png

usually PLL2_PFD0 is used by LVDS. LVDS clock is not expected to be changed. If there is no any other module which used PLL2_PFD0, VPU clock can be configured to use PLL2_PFD0.

0 项奖励
回复