About audio: how do I ensure which internal aux port is used

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

About audio: how do I ensure which internal aux port is used

1,268 次查看
kainanzhu
Contributor I

Hi NXP:

   I'm now porting audio. I used external  aux port is aux3 from Schematic, but I don't know which internal port is used.

   How do I ensure which internal aux port is used?

  

Thanks.

0 项奖励
回复
7 回复数

1,128 次查看
diegoadrian
NXP Employee
NXP Employee

Hello,

Are you using one of our boards? If yes, Which one?

Best Regards,

Diego.

0 项奖励
回复

1,128 次查看
kainanzhu
Contributor I

Hi:

   Yes, I use imx6q.

Thanks

0 项奖励
回复

1,128 次查看
kainanzhu
Contributor I

Yes. I'm using the SABRESD board

0 项奖励
回复

1,128 次查看
diegoadrian
NXP Employee
NXP Employee

Hello

Like you said, according to the schematic, the external aux port is connected to aud3 port. But following the schematic that audio port is connected to the CSI0_DAT (4 - 7) of the i.MX6Q - DISP CSI. Confirming with the i.MX pins tool the CSI0_DAT (4 - 7) is muxed with the AUD3_TXC, AUD3_TXD, AUD3_TXFS, AUD3_RXD respectively.

I hope this can solve your question.

Best Regards,

Diego.

0 项奖励
回复

1,128 次查看
diegoadrian
NXP Employee
NXP Employee

Hello

Are you using the SABRESD board?

Best Regards,

Diego.

0 项奖励
回复

1,128 次查看
kainanzhu
Contributor I

Hi Vaverka:

   we use imx6qdl.

Thanks.

0 项奖励
回复

1,128 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Kainan,

Could you please specify which NXP IC are you using? It will help us to find the correct space for your question.

Best regards,

Tomas

0 项奖励
回复