About VCOIN register setting for MMPF0100

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About VCOIN register setting for MMPF0100

Jump to solution
975 Views
george
Senior Contributor II

Dear all,

I want to adjust the voltage for charging from PMIC (MMPF0100F0AEP) to Li-Battery.

Though VCOIN [2:0] (ADDR 0x1A) was changed to 100 from 000, It seems that the voltage to LICELL pin does not change.

If the register value is read, it is changed correctly.

Is anything else needed?

Best Regards,

George

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
810 Views
igorpadykov
NXP Employee
NXP Employee

Hi George

additionaly one needs to set bit COINCHEN=1

and check that VIN > UVDET (3.1v) sect.6.4.7.1Coin Cell Battery Backup

MMPF0100

Also charger behaves as current-limited voltage source, resulting in the CC/CV

taper characteristic. If you cannected licell with small internal resistance,

it is difficult to see change. One can try to imitate licell connecting 50kOhm resistance

(50K*60uA=3.0V) and check voltage on it.

Best regards

igor

View solution in original post

0 Kudos
Reply
2 Replies
811 Views
igorpadykov
NXP Employee
NXP Employee

Hi George

additionaly one needs to set bit COINCHEN=1

and check that VIN > UVDET (3.1v) sect.6.4.7.1Coin Cell Battery Backup

MMPF0100

Also charger behaves as current-limited voltage source, resulting in the CC/CV

taper characteristic. If you cannected licell with small internal resistance,

it is difficult to see change. One can try to imitate licell connecting 50kOhm resistance

(50K*60uA=3.0V) and check voltage on it.

Best regards

igor

0 Kudos
Reply
810 Views
george
Senior Contributor II

Dear Igor,

Thank you for explanation carefully.

BR,

Geroge

0 Kudos
Reply