About VBUS voltage supply in Power-up for i.MX6Dual Lite

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About VBUS voltage supply in Power-up for i.MX6Dual Lite

Jump to solution
1,411 Views
yuuki
Senior Contributor II

Dear all,

By our system, the voltage is applied into Pin E9 USB_OTG_VBUS by the outside during power-up sequence of i.MX6DL.
The moment current is 64mA.
Afterwards, 10mA flows during 62msec.

Does this give damage in i.MX6DL?
may i.MX6DL be broken by this?

Best Regards,
Yuuki

Labels (1)
Tags (1)
0 Kudos
1 Solution
1,131 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

it does not conflict to data sheet, if you wish to

comply with the USB OTG specification, one should follow its requirements.

Still, hardware endures and works fine in case when USB_OTG_VBUS 

is powered at any time.

Best regards
igor

View solution in original post

0 Kudos
3 Replies
1,131 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

according to sect.4.2.1 Power-Up Sequence i.MX6SDL Datasheet:

USB_OTG_VBUS and USB_H1_VBUS are not part of the power supply
sequence and may be powered at any time.

http://www.nxp.com/docs/en/data-sheet/IMX6SDLCEC.pdf 

So this will not damage i.MX6DL.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
1,131 Views
yuuki
Senior Contributor II

igorpadykov

Dear Igor-san,

Thank you for your quick quick response.

I found the following explanation in Hardware Development Guide.
I think that it conflicts to the explanation of the data sheet.

How should I understand it?

<Hardware Development Guide>
1. USB OTG
To comply with the USB OTG specification, the VBUS supply on the OTG connector should default to off when the boards power up.

Best Regards,
Yuuki

0 Kudos
1,132 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

it does not conflict to data sheet, if you wish to

comply with the USB OTG specification, one should follow its requirements.

Still, hardware endures and works fine in case when USB_OTG_VBUS 

is powered at any time.

Best regards
igor

0 Kudos