About Support RTL8188 8192 wifi dongle in FSL JB4.2.2-GA release

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

About Support RTL8188 8192 wifi dongle in FSL JB4.2.2-GA release

1,520 次查看
david5icp
Contributor III

Hello ~Good Day!

I follow Support RTL8188 8192 wifi dongle in FSL JB4.2.2-GA release  to build RTL8188 driver on Android 4.2.2 GA. But i can't get "kernel_imx/net/wireless/cfg80211.ko" on my project. How do i to get that ?

And if I by pass "cfg80211.ko", i got message as below::

-------------------------------------------------------------------------------------------------------

Install USB Dongle::

usb 2-1.1: New USB device found, idVendor=0bda, idProduct=8179

usb 2-1.1: New USB device strings: Mfr=1, Product=2, SerialNumber=3

usb 2-1.1: Product: 802.11n NIC

usb 2-1.1: Manufacturer: Realtek

usb 2-1.1: SerialNumber: 8C18D916247D

------------------------------------------------------------------------------------------------------

After 3 seconds::

usbcore: registered new interface driver rtl8192cu

usb usb1: usb auto-resume

ehci_fsl_bus_resume begins, DR

usb usb1: bus resume fail, err -108

usbcore: deregistering interface driver rtl8192cu

------------------------------------------------------------------------------------------------------

I got it and registered, but deregistering in coming  few seconds...

Does it correct ? How do i do ? Thanks!

BR

David

标签 (2)
0 项奖励
回复
2 回复数

1,060 次查看
igorpadykov
NXP Employee
NXP Employee

Hi David

for cfg80211.ko issue one can check

Want to port wifi driver to imx28evk.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,060 次查看
david5icp
Contributor III

Hi Igor,

Yes, I cat create "cfg80211.ko" now. But RTL8188 dongle still now working, and deregistering in coming  few seconds...

And I can't  "wlan0".

---------------------------------------------------------------------------------------------------------

usb 2-1.1: New USB device found, idVendor=0bda, idProduct=8179

usb 2-1.1: New USB device strings: Mfr=1, Product=2, SerialNumber=3

usb 2-1.1: Product: 802.11n NIC

usb 2-1.1: Manufacturer: Realtek

usb 2-1.1: SerialNumber: 8C18D916247D

usb 2-1.1: usb_probe_device

usb 2-1.1: configuration #1 chosen from 1 choice

usb 2-1.1: adding 2-1.1:1.0 (config #1, interface 0)

usbserial_generic 2-1.1:1.0: usb_probe_interface

usbserial_generic 2-1.1:1.0: usb_probe_interface - got id

drivers/usb/core/inode.c: creating file '003'

hub 2-1:1.0: port 2, status 0301, change 0000, 1.5 Mb/s

Freeing init memory: 224K

usb 2-1.2: link qh8-0601/cc09bd60 start 2 [1/2 us]

flexcan imx6q-flexcan.0: writing ctrl=0x03292005

usb 2-1.2: unlink qh8-0601/cc09bd60 start 2 [1/2 us]

fsl-ehci fsl-ehci.1: reused qh cc09bd60 schedule

usb 2-1.2: link qh8-0601/cc09bd60 start 2 [1/2 us]

usb 2-1.2: unlink qh8-0601/cc09bd60 start 2 [1/2 us]

fsl-ehci fsl-ehci.1: reused qh cc09bd60 schedule

usb 2-1.2: link qh8-0601/cc09bd60 start 2 [1/2 us]

usb 2-1.2: unlink qh8-0601/cc09bd60 start 2 [1/2 us]

warning: `zygote' uses 32-bit capabilities (legacy support in use)

fsl-ehci fsl-ehci.1: reused qh cc09bd60 schedule

usb 2-1.2: link qh8-0601/cc09bd60 start 2 [1/2 us]

usbcore: registered new interface driver rtl8192cu

acc_open

acc_release

usb usb1: usb auto-resume

ehci_fsl_bus_resume begins, DR

usb usb1: bus resume fail, err -108

sys_prop: permission denied uid:1003  name:service.bootanim.exit

usbcore: deregistering interface driver rtl8192cu

---------------------------------------------------------------------------------------------------------

BR.

David

0 项奖励
回复