Dear All,
The difference was seen STCK and STFS value between Expected and Observed in i.MX6DQ.
Could you tell me the correct setting?
(Device: i.MX6Quad, BSP: L3.14.28)
*Refer to attached file.
======
[Output Result]
STFS:
(Expected value) 44.1kHz
(Observed value) 33.07kHz
STCK:
(Expected value) 2.1156MHz
(Observed value) 2.12MHz
[Input]
pll4_main_clk : 169.344MHz
[Register Setting]
SSI1_STCCR
-DIV2 0b
-PSR 0b
-WL 1011b (Number of Bits = 24)
-DC 00001b
-PM 000 0000b (Divide by 1)
======
Best Regards,
Keita
Solved! Go to Solution.
Hello Keita,
See following , please! The reply is from i.MX Expert team:
t looks like correct in the register settings. But I want to know how the customer to modify the registers and how the customer to use the SSI driver?
In general we only need to pre-caculated which frequency point we need and just set it in Linux driver. For example, for 44.1KHz output, we may configure SSI root clock to 22.5792MHz ( it is a classical frequecy point) and we can calculated PLL4 to 180.6336MHz.
clk_set_rate(&pll4_audio_main_clk, 180633600);
clk_set_parent(&ssi2_clk, &pll4_audio_main_clk);
clk_set_rate(&ssi2_clk, 22579200);
Then we can configure our SSI driver to use 44.1KHz clock and the driver can automatically set the related registers.
Regards,
Weidong
Hello Keita,
The cusotmer's operation is correct, but I can't confirm what happened, so I submitted the question to i.MX expert team, Let us wait for their reply!
Regards,
Weidong
Hello Keita,
See following , please! The reply is from i.MX Expert team:
t looks like correct in the register settings. But I want to know how the customer to modify the registers and how the customer to use the SSI driver?
In general we only need to pre-caculated which frequency point we need and just set it in Linux driver. For example, for 44.1KHz output, we may configure SSI root clock to 22.5792MHz ( it is a classical frequecy point) and we can calculated PLL4 to 180.6336MHz.
clk_set_rate(&pll4_audio_main_clk, 180633600);
clk_set_parent(&ssi2_clk, &pll4_audio_main_clk);
clk_set_rate(&ssi2_clk, 22579200);
Then we can configure our SSI driver to use 44.1KHz clock and the driver can automatically set the related registers.
Regards,
Weidong
Hi Weidong,
Sorry for my delay response.
I could confirm that my customer got the correct frequency!
Thank you very much.
Best Regards,
Keita
Hi Weidong,
Thank you for your reply.
OK. I'll confirm it and feedback you.
Best Regards,
Keita
Hello Keita,
According to your description, I calculated it like this: 48 x STFS = STCK, that is 48 x 44.1k = 2.1168MHz, So your STCK should be 2.1168MHz. But now the value you measured is 2.12MHz, I feel the STCK can be considered as correct one.
According to above calculating method, if we want to get correct STFS, we should make STCK devided by 48, so please try to configure it !
Regards,
Weidong
Hi Weidong,
Do you have any update?
Best Regards,
Keita
Hi Weidong,
Thank you for your reply.
According to above calculating method, if we want to get correct STFS,
we should make STCK devided by 48, so please try to configure it !
Refer to excel sheet again.
My customer had already set the STCK divided by 48.