About SPI-I/F control for MX28.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About SPI-I/F control for MX28.

跳至解决方案
1,924 次查看
george
Senior Contributor II

Dear All,

Currently, my customer is developing the product using i.MX287.

Their board has SPI-SRAM.

It is connected by using SSP as SPI-Master mode.

Though SPI access works correctly, it halts operation rarely.

Their program waits for HW_SSP_CTRL0_RUN bit = 0, in order to check whether transfer was completed or not.

However, it is not rarely set to 0.

Is polling HW_SSP_CTRL0_RUN bit = 0 correct in order to detect the completion of transfer?

Please let me know if you came up with something our mistake.

Best Regards,

George

标签 (3)
0 项奖励
回复
1 解答
1,539 次查看
igorpadykov
NXP Employee
NXP Employee

Hi George

polling bit HW_SSP_CTRL0_RUN  is correct for checking

whether transfer was completed or not. One can look at SPI-NOR patches

where this is used.

How to enable SPI NOR boot for i.MX28 (Spansion s25fl256s)

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
6 回复数
1,540 次查看
igorpadykov
NXP Employee
NXP Employee

Hi George

polling bit HW_SSP_CTRL0_RUN  is correct for checking

whether transfer was completed or not. One can look at SPI-NOR patches

where this is used.

How to enable SPI NOR boot for i.MX28 (Spansion s25fl256s)

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,539 次查看
george
Senior Contributor II

Dear Igor,

My customer had already referred to above-mentioned patch for the SPI access sequence.

They did continuous write test to connected SPI-SRAM.

It works almost correctly, but the access hangs very rarely.

According to their investigation, in the following, it keeps being HW_SSP_CTRL0_RUN bit = 1.

*HW_SSP_CTRL0_RUN bit  is not set to 0.

while( HW_SSP_CTRL0_RD( m_Index ) & BM_SSP_CTRL0_RUN ) {

}

And then they have found not seeing the symptoms by reading a status register as follow.

volatile UINT32 tmp ;

while( HW_SSP_CTRL0_RD( m_Index ) & BM_SSP_CTRL0_RUN ) {

     tmp = HW_SSP_STATUS_RD( m_Index ) ;

}

Is this workaround available?

I recommended to take in a timeout mechanism which is in linux-code as follow.

count = 10000;

while ((__raw_readl(ss->regs + HW_SSP_CTRL0) & BM_SSP_CTRL0_RUN)

       && count--)

        continue;

if (count <= 0) {

        printk(KERN_ERR "%c: timeout on line %s:%d\n",

               write ? 'W' : 'C', __func__, __LINE__);

        break;   

}

What should we do with the recovery sequence when being timeout?

*I can not find it in linux-code.

Best regards,

George

0 项奖励
回复
1,539 次查看
igorpadykov
NXP Employee
NXP Employee

Hi George

seems one can try to reset SSP

Best regards

igor

0 项奖励
回复
1,539 次查看
george
Senior Contributor II

Dear Igor,

What do you think about the way of poling RUN bit and reading STATUS register?

Thnaks,

George

0 项奖励
回复
1,539 次查看
igorpadykov
NXP Employee
NXP Employee

Hi George

for its usage one can look at SPI-NOR patches in first answer.

Best regards

igor

0 项奖励
回复
1,539 次查看
george
Senior Contributor II

Dear Igor,

I tell my customer checking it.

Thanks,

George

0 项奖励
回复