Dear All,
Hello. Now, my customer is considering to use the QSPI for FPGA connection.
[Q1]
Is it possible to use the QSPI for FPGA?
And, Is a QSPI driver prepared for FPGA?
[Q2]
When transferring the data using DMA, Is it possible to send the data without becoming Buffer Full of FIFO?
BSP:L3.14.28_1.0.0
Best Regards,
Keita
解決済! 解決策の投稿を見る。
Hi Keita
>[Q1]Is it possible to use the QSPI for FPGA?
yes.
>And, Is a QSPI driver prepared for FPGA?
no
>[Q2]When transferring the data using DMA, Is it possible to send
>the data without becoming Buffer Full of FIFO?
yes, behavior depends on QuadSPIx_RBCT[WMRK] setting
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Keita
>[Q1]Is it possible to use the QSPI for FPGA?
yes.
>And, Is a QSPI driver prepared for FPGA?
no
>[Q2]When transferring the data using DMA, Is it possible to send
>the data without becoming Buffer Full of FIFO?
yes, behavior depends on QuadSPIx_RBCT[WMRK] setting
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------