About MediaCodec API on Android4 .4.3 with i.MX6Q-SABRE-SDB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About MediaCodec API on Android4 .4.3 with i.MX6Q-SABRE-SDB

跳至解决方案
1,590 次查看
yuuki
Senior Contributor II

Dea all,

We run Android4.4.3 BSP on i.MX6Q-SABRE-SDB board.

We want to decode WMV video file by using MediaCodec API.

However, WMV file does not be decoded.

We suspect that MediaCodec API cannot call HW Video Codec of i.MX6.

Can MediaCodec API call HW codec of i.MX6 for WMV decoding?

Would you tell me the method if it is possible?

May I have advice?

Best Regards,

Yuuki

标签 (2)
标记 (3)
0 项奖励
1 解答
1,392 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

support for restricted distribution codec package

is provided as confidentional , please elevate it with local fae.

Best regards

igor

在原帖中查看解决方案

0 项奖励
5 回复数
1,392 次查看
saurabh206
Senior Contributor III

Hi

i.MX6 supports HW decoding of WMV.

I think WMV library is not openly available , you need to contact Local FAE.

Thanks

Saurabh

1,392 次查看
yuuki
Senior Contributor II

Dea Saurabh-san,

Thank you for your quick response.

Do you mean omxplayer_source?

If so, we have already got this from your Loacal FAE.

We suspect that MediaCodec API does not support WMV because WMV library is not openly available.

Best Regards,

Yuuki

0 项奖励
1,392 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

WMV codecs are restricted distribution codec package,

distribution is done via controlled access extranet site and requires

agreement to be in place with Microsoft. Please refer to attached

Extended Codec Release Notes p.3, 9.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

1,392 次查看
yuuki
Senior Contributor II

Dear Igor-san,

Thank you for your support.

I think that you show fsl_ms_codec.tar.gz package.

We have already installed this package.

May I understand that MediaCodec API does not support WMV?

Best Regards,

Yuuki

0 项奖励
1,393 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

support for restricted distribution codec package

is provided as confidentional , please elevate it with local fae.

Best regards

igor

0 项奖励