Hi There,
I want to check for IMX6.
Unused MIPI recommends "Leave unconnected".
Hardware Development Guide for i.MX 6DualPlus/6QuadPlus, 6Dual/6Quad and i.MX 6Solo/6DualLite Applications Processors
2.8 Unused analog interfaces
Is this due to shutting down the PHY?
We are considering whether termination is necessary when the camera is not in use.
Is it possible to terminate (for internal IMX6) MIPI CSI?
Do I have to terminate externally?
Best regards
- satoshi
已解决! 转到解答。
Hello
Please just follow recommendations of the Hardware Development Guide :
no need for termination of the mentioned signals.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
Hello
Please just follow recommendations of the Hardware Development Guide :
no need for termination of the mentioned signals.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!