Dear All,
I refer to the following part of a reference manual.
http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf
- Table 23-130. Receive FIFO thresholds definition(P.1189)
"MAC status signal" is described here.
However, I cannot find explanation about this MAC status signal.
What does this signal show concretely?
Best Regards,
Yuuki
已解决! 转到解答。
The MAC status signal is internal one of ENET module.
For programming please use status bits, available in Interrupt
Event Register (ENET_EIR).
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
The MAC status signal is internal one of ENET module.
For programming please use status bits, available in Interrupt
Event Register (ENET_EIR).
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------