About MAC status signal of ENET of i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About MAC status signal of ENET of i.MX6

Jump to solution
813 Views
yuuki
Senior Contributor II

Dear All,

I refer to the following part of a reference manual.
http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf
- Table 23-130. Receive FIFO thresholds definition(P.1189)

"MAC status signal" is described here.
However, I cannot find explanation about this MAC status signal.

What does this signal show concretely?

Best Regards,
Yuuki

Labels (1)
0 Kudos
Reply
1 Solution
720 Views
Yuri
NXP Employee
NXP Employee

  The MAC status signal is internal one of ENET module.
For programming please use status bits, available in Interrupt
Event Register (ENET_EIR).

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
721 Views
Yuri
NXP Employee
NXP Employee

  The MAC status signal is internal one of ENET module.
For programming please use status bits, available in Interrupt
Event Register (ENET_EIR).

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply