Dear all,
We'll connect a LCD panel.
In MX6DL_SABRE-SDP, there are the following control signals.
DI0_PIN2 => DISP0_HSYNCH
DI0_PIN3 => DISP0_VSYNCH
DI0_PIN4 => DISP0_CNTRST
DI0_PIN15 => DISP0_DRDY
These signals aren't explained in "Pin Assignments" of a reference manual(IMX6SDLRM.pdf).
However, in IOMUX tool, these signals are assigned to ALT1 mode.
Can these signals be used in ALT1 mode?
Or is the GPIO function used as these signals?
Best Regards,
Yuuki
解決済! 解決策の投稿を見る。
Hi yuuki
in Linux DI0_PIN2,3,15 are used in ALT0 mode as
IPUa_DIb_PINcd, one can look at ipu_disp.c.
I think it is not possible to produce IPU sync signals with GPIO
configurations.
Seems DI0_PIN4 DISP0_CNTRST is used as GPIO (ALT5).
Probably for these signals IOMUX tool has some inaccuracies.
Best regards
igor
Hi yuuki
in Linux DI0_PIN2,3,15 are used in ALT0 mode as
IPUa_DIb_PINcd, one can look at ipu_disp.c.
I think it is not possible to produce IPU sync signals with GPIO
configurations.
Seems DI0_PIN4 DISP0_CNTRST is used as GPIO (ALT5).
Probably for these signals IOMUX tool has some inaccuracies.
Best regards
igor