About REGx_ADJ of PMU_REG_CORE of i.MX6Solo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About REGx_ADJ of PMU_REG_CORE of i.MX6Solo

Jump to solution
972 Views
yuuki
Senior Contributor II

Dear all,

We refer to Description in REGx_ADJ field of PMU_REG_CORE register.

IMX6SDLRM.pdf:
- 51.7.1 Digital Regulator Core Register (PMU_REG_CORE)(P.4522)

REGx_ADJ=0000 is "No adjustment".

In what kind of case is setting of REGx_ADJ=0000 used?

May I have advice?

Best Regards,
Yuuki

Labels (1)
0 Kudos
Reply
1 Solution
871 Views
igorpadykov
NXP Employee
NXP Employee

Hi yuuki

REGx_ADJ=0000 means default, as

IMX6SDLRM p.4517 describes:

The target voltages of these regulators are all reset to 1.1 V on startup.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
872 Views
igorpadykov
NXP Employee
NXP Employee

Hi yuuki

REGx_ADJ=0000 means default, as

IMX6SDLRM p.4517 describes:

The target voltages of these regulators are all reset to 1.1 V on startup.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply