About LCD IF max resolution of i.MX6UL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About LCD IF max resolution of i.MX6UL

跳至解决方案
1,136 次查看
yuuki
Senior Contributor II

Dear all,

The parallel display port of i.MX6UL supports resolution of maximum WXGA (1366 x 768).

We need resolution of 1280 x 800.

Can display port support resolution of 1280 x 800?

Best Regards,

Yuuki

标签 (1)
0 项奖励
回复
1 解答
890 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

yes it can support, probably with slower fps, as there are

no hardware limitations limited only to WXGA.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
891 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

yes it can support, probably with slower fps, as there are

no hardware limitations limited only to WXGA.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
890 次查看
shanashiro
Contributor I

Dear all,

How to calculte fps when resolution of 1280 x 800 ?

Best Regards,
Seiso

0 项奖励
回复