About LCD IF max resolution of i.MX6UL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About LCD IF max resolution of i.MX6UL

Jump to solution
1,132 Views
yuuki
Senior Contributor II

Dear all,

The parallel display port of i.MX6UL supports resolution of maximum WXGA (1366 x 768).

We need resolution of 1280 x 800.

Can display port support resolution of 1280 x 800?

Best Regards,

Yuuki

Labels (1)
0 Kudos
Reply
1 Solution
886 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

yes it can support, probably with slower fps, as there are

no hardware limitations limited only to WXGA.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
887 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

yes it can support, probably with slower fps, as there are

no hardware limitations limited only to WXGA.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
886 Views
shanashiro
Contributor I

Dear all,

How to calculte fps when resolution of 1280 x 800 ?

Best Regards,
Seiso

0 Kudos
Reply