About IMX8M 604 Ohm Termination Resistors

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About IMX8M 604 Ohm Termination Resistors

499件の閲覧回数
yurdakulTR
Contributor I

Hi NXP Support Team, 

        I am designing a project using Variscite Dart-MX8M SOM based on NXP IMX8M. Variscite adds 604Ohm termination resistors for the HDMI part on the SOM development board. Additionally, I have seen these termination resistors in your evaluation kit schematics. Are these resistors a must? Is it a problem if we don't add them? I am waiting for your feedback? Thanks. 

0 件の賞賛
返信
2 返答(返信)

478件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

According to the Hardware Developer’s Guide, 604Ω resistors are needed for stable HDMI operation.

Best regards.

0 件の賞賛
返信

326件の閲覧回数
yurdakulTR
Contributor I

Hi, 

         Thanks for answer. 

Best regards. 

 

0 件の賞賛
返信