Hi There,
I want to check for IMX7 Dual.
I obtained IBIS model for implementing the SI simulation.
SI:Signal Integrity
Memory uses LPDDR3.
IBIS models has the following two models.
・mx7d_12x12_1p8v_lpddr3.ibs
・mx7d_12x12_3p3v_lpddr3.ibs
I use IMX7 Dual.
Device:「MCIMX7D7DVM10SC」
Do you have a model of 19x19?
Best regards
- satoshi
解決済! 解決策の投稿を見る。
Hello,
Please refer to Table 27 (IBIS Model naming convention) of the Hardware Development Guide
Different IBIS files relate to different GPIO supply voltages NVCC_xxx.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
Please refer to Table 27 (IBIS Model naming convention) of the Hardware Development Guide
Different IBIS files relate to different GPIO supply voltages NVCC_xxx.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi, Yuri
Thank you for your reply.
Best regards
- satoshi
Hi There,
Sorry, Model was incorrect.
19x19 model was available.
I want to check for IMX7 Dual.
I obtained IBIS model for implementing the SI simulation.
SI:Signal Integrity
Memory uses LPDDR3.
IBIS models has the following two models.
・mx7d_19x19_1p8v_lpddr3.ibs
・mx7d_19x19_3p3v_lpddr3.ibs
How should used properly of model ?
Should I change the model in the case of somewhere voltage 1.8V or 3.3V ?
Best regards
- satoshi