Dear All,
Hello. I have a question about G2D API.
Refer to Chapter 2 i.MX 6 G2D API in "i.MX_6_Graphics_User's_Guide.pdf".
Could you give me below information?
- Header file to include
- Library to link
Best Regards,
Keita
解決済! 解決策の投稿を見る。
Hello,
"There are two ways to see the g2d test source,
1. If you have the vivante license to have vivante gpu source code, you can see the code in gpu-viv(5)/fsl_drv/g2d, there are scripts to build the g2d_test and g2d_overlay_test.
2. If you don't have the license to have vivante gpu source code, the g2d_test and g2d_overlay_test have been integrated into new demo framework. It is the C++ framework, but g2d_test and g2d_overlay_test keeps the same as in driver, they just have C++ wrap. The code is in /your yocto directory build director something like
/yocto-ga-wayland/build-wayland/tmp/work/cortexa9hf-vfp-neon-mx6qdl-poky-linux-gnueabi/fsl-gpu-sdk/2.2.1-r0/fsl-gpu-sdk-2.2.1/DemoApps/G2D
There are detailed instruction to build these apps stand alone in yocto-ga-wayland/build-wayland/tmp/work/cortexa9hf-vfp-neon-mx6qdl-poky-linux-gnueabi/fsl-gpu-sdk/2.2.1-r0/fsl-gpu-sdk-2.2.1/Doc/Setup_guide_yocto.txt"
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
Please refer to section 8 (Graphics) of "i.MX_Linux_User's_Guide.pdf".
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Yuri,
Thank you for your quick reply.
I referred to section 8 (Graphics) of "i.MX_Linux_User's_Guide.pdf".
Where are header file and linked library of G2D API?
Best Regards,
Keita
Hello,
"There are two ways to see the g2d test source,
1. If you have the vivante license to have vivante gpu source code, you can see the code in gpu-viv(5)/fsl_drv/g2d, there are scripts to build the g2d_test and g2d_overlay_test.
2. If you don't have the license to have vivante gpu source code, the g2d_test and g2d_overlay_test have been integrated into new demo framework. It is the C++ framework, but g2d_test and g2d_overlay_test keeps the same as in driver, they just have C++ wrap. The code is in /your yocto directory build director something like
/yocto-ga-wayland/build-wayland/tmp/work/cortexa9hf-vfp-neon-mx6qdl-poky-linux-gnueabi/fsl-gpu-sdk/2.2.1-r0/fsl-gpu-sdk-2.2.1/DemoApps/G2D
There are detailed instruction to build these apps stand alone in yocto-ga-wayland/build-wayland/tmp/work/cortexa9hf-vfp-neon-mx6qdl-poky-linux-gnueabi/fsl-gpu-sdk/2.2.1-r0/fsl-gpu-sdk-2.2.1/Doc/Setup_guide_yocto.txt"
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear Yuri,
Thank you for great information!
Best Regards,
Keita