About ERR004365 EXSC: Exclusive accesses to certain memories are not supported to full AXI specification in i.MX6DQ.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About ERR004365 EXSC: Exclusive accesses to certain memories are not supported to full AXI specification in i.MX6DQ.

ソリューションへジャンプ
646件の閲覧回数
keitanagashima
Senior Contributor I

Dear All,

Refer to ERR004365 in IMX6DQCE(Rev.6).

Projected Impact is "EIM does not support exclusive accesses according to AXI specifications."

[Questions]

1. Is there a use case of exclusive accesses in BSP (jb4.2.2_1.0.0)?

2. I think that the user doesn't need to care the AXI bus access.

How implement the workaround to avoid the exclusive accesses?

Best Regards,

Keita

ラベル(3)
0 件の賞賛
返信
1 解決策
559件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  ARM provides exclusive access functionality via the LDREX/STREX pair of instructions.

ARM Information Center

NXP Android does not use this mechanism for EIM.  

To avoid the issue customers also should not use these exclusive accesses for EIM in their

applications and drivers.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
560件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  ARM provides exclusive access functionality via the LDREX/STREX pair of instructions.

ARM Information Center

NXP Android does not use this mechanism for EIM.  

To avoid the issue customers also should not use these exclusive accesses for EIM in their

applications and drivers.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信