Dear All,
Hello.
First, refer to Table 20-6. AXI Burst Cycles Supported in IMX6SLRM(Rev.2).
It looks support only 16 word.
Next, refer to "BL" bits of 20.9.1 Chip Select n General Configuration Register 1 (EIM_CSnGCR1) in IMX6SLRM(Rev.2).
The description looks 32 words setting can be set.
Why did look the difference?
Best Regards,
Keita
已解决! 转到解答。
Hi Keita
you are right there is difference, because EIM and AXI bus
IP modules were developed independently and before i.MX6SL design.
These IP blocks are used in many processors.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Keita
you are right there is difference, because EIM and AXI bus
IP modules were developed independently and before i.MX6SL design.
These IP blocks are used in many processors.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------