Dear All,
Hello. I have questions about EIM burst access in i.MX6SL.
My customer will connect the FPGA via EIM on custom board and want to fix the FPGA's output timing.
[Q1] About Burst Read Memory Accesses
Refer to "20.8.7 Burst (Synchronous Mode) Read Memory Accesses Timing Diagram - BCD=0" in i.MX 6SoloLite Applications Processor Reference Manual, Rev. 2, 06/2015.
Is my below understanding right?
- Latch timing of control signals by FPGA is rising edge of BCLK.
- Output read data timing is falling edge of BCLK.
[Q2] About Burst Write Memory Accesses
Refer to "20.8.9 Burst (Synchronous Mode) Write Memory Access Timing - BCD=1" in i.MX 6SoloLite Applications Processor Reference Manual, Rev. 2, 06/2015.
Is my below understanding right?
- Latch timing of all signals (control & data) by FPGA is rising edge of BCLK.
[Q3]
I think that the register to select the BCLK polarity (rising or falling) doesn't exist in i.MX6SL.
Is it right?
Best Regards,
Keita
已解决! 转到解答。
Hello,
1.
According to the i.MX6SL Datasheet : “All EIM output control
signals may be asserted and deasserted by an internal clock synchronized
to the BCLK rising edge according to corresponding assertion/negation control
fields.”
For data, from the Datasheet, table “EIM Bus Timing Parameters”, parameters
WE18 - Input data setup time to clock rise
WE19 - Input data hold time from clock rise
So, again, the rising edge is used.
2.
For data, from the Datasheet, table “EIM Bus Timing Parameters”, parameters
WE16 - Clock rise to output data valid
WE17 - Clock rise to output data invalid
Rising edge is used.
3.
Correct : “ […] the register to select the BCLK polarity (rising or falling) doesn't
exist in i.MX6SL.”
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
1.
According to the i.MX6SL Datasheet : “All EIM output control
signals may be asserted and deasserted by an internal clock synchronized
to the BCLK rising edge according to corresponding assertion/negation control
fields.”
For data, from the Datasheet, table “EIM Bus Timing Parameters”, parameters
WE18 - Input data setup time to clock rise
WE19 - Input data hold time from clock rise
So, again, the rising edge is used.
2.
For data, from the Datasheet, table “EIM Bus Timing Parameters”, parameters
WE16 - Clock rise to output data valid
WE17 - Clock rise to output data invalid
Rising edge is used.
3.
Correct : “ […] the register to select the BCLK polarity (rising or falling) doesn't
exist in i.MX6SL.”
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------