About DQ amplitude by DDR3 stress test in i.MX6DQ.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About DQ amplitude by DDR3 stress test in i.MX6DQ.

ソリューションへジャンプ
875件の閲覧回数
keitanagashima
Senior Contributor I

Dear All,

Hello. We found the 1st bit of the DQ amplitude was small by DDR3 stress test (Writing mode).

And, tDS/tDQ found tight specifications (DQS or DQ - CLK).

*Refer to attached file.

How to increase the DQ amplitude?

For example, if user increase the DQ Drive strength (40 Ohm --> 34Ohm), is this issue improved?

This question is related to the following thread.

https://community.freescale.com/message/558926#558926

Best Regards,

Keita

ラベル(2)
0 件の賞賛
返信
1 解決策
722件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

Yes, the DQ amplitude may be improved by increasing the drive strength.

Regards,

Yuri.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
722件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Please refer to reply from app team in

About Signal amplitude on DQ lines in i.MX6DQ.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
722件の閲覧回数
keitanagashima
Senior Contributor I

Dear Yuri,

Hello. Thank you for your reply.

I think so, too.

The amplitude was improved by ODT setting.

Another way, the DQ amplitude was improved by increasing the drive strength, isn't it?

Best Regards,

Keita

0 件の賞賛
返信
723件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

Yes, the DQ amplitude may be improved by increasing the drive strength.

Regards,

Yuri.

0 件の賞賛
返信