About DQ amplitude by DDR3 stress test in i.MX6DQ.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About DQ amplitude by DDR3 stress test in i.MX6DQ.

Jump to solution
1,017 Views
keitanagashima
Senior Contributor I

Dear All,

Hello. We found the 1st bit of the DQ amplitude was small by DDR3 stress test (Writing mode).

And, tDS/tDQ found tight specifications (DQS or DQ - CLK).

*Refer to attached file.

How to increase the DQ amplitude?

For example, if user increase the DQ Drive strength (40 Ohm --> 34Ohm), is this issue improved?

This question is related to the following thread.

https://community.freescale.com/message/558926#558926

Best Regards,

Keita

Labels (2)
0 Kudos
Reply
1 Solution
864 Views
Yuri
NXP Employee
NXP Employee

Hello,

Yes, the DQ amplitude may be improved by increasing the drive strength.

Regards,

Yuri.

View solution in original post

0 Kudos
Reply
3 Replies
864 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please refer to reply from app team in

About Signal amplitude on DQ lines in i.MX6DQ.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
864 Views
keitanagashima
Senior Contributor I

Dear Yuri,

Hello. Thank you for your reply.

I think so, too.

The amplitude was improved by ODT setting.

Another way, the DQ amplitude was improved by increasing the drive strength, isn't it?

Best Regards,

Keita

0 Kudos
Reply
865 Views
Yuri
NXP Employee
NXP Employee

Hello,

Yes, the DQ amplitude may be improved by increasing the drive strength.

Regards,

Yuri.

0 Kudos
Reply