Hi community.
Our customer has below question.
About DMA of ECSPI,
ECSPI by Configu to SPI of the Master, so it is to transmit only.
( Receive is not performed).
TXFIFO side, as to send data using DMA,
RXFIFO side, ignoring overflow, sending doesn't matter?
(For example, Disable to RXFIFO Overflow Interrupt , do not affect the TX processing?)
已解决! 转到解答。
Hi Takashi
you are right, RX side can be ignored, possibly disabling
RXFIFO Overflow Interrupt. This should not affect TX processing.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Takashi
you are right, RX side can be ignored, possibly disabling
RXFIFO Overflow Interrupt. This should not affect TX processing.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------