Dear All,
My customer downloaded the MFG tool Source (mfgtool.v2.3.2.SRC).
Is it possible to build it by Visual Studio 2015?
(They tried to build it on Visual Studio 2015. But, the result was error.)
- Windows SDK v7.1 didn't linked with Visual Studio 2015.
- Error message appeared like a "No Visual Studio 2008"
[Build Requirements from mfgtool.v2.3.2.SRC document]
Tools:
• Visual Studio 2008 Professional
• Windows 7 WDK 7600.16385.0 or later, 7600.16385.1 is better
• Windows SDK v6.0A or later, v7.1 is better
Best Regards,
Keita
Solved! Go to Solution.
Hello,
I have some doubt if other than VS2008 version may be easy used for MFG
build, since only relatively simple applications can be rebuild for different VS
versions without modifications. Often special import tool should be applied
to import an application from previous release of VS. But for the VS2015
already several releases were issued.
Basically You could use only (C) sources to create new project, but I am afraid
problems may take place when using Windows SDK and WDK.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
I have some doubt if other than VS2008 version may be easy used for MFG
build, since only relatively simple applications can be rebuild for different VS
versions without modifications. Often special import tool should be applied
to import an application from previous release of VS. But for the VS2015
already several releases were issued.
Basically You could use only (C) sources to create new project, but I am afraid
problems may take place when using Windows SDK and WDK.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------