Hi all,
i need help about ".apk" file installation in iMX508 running Android
Could somebody tell how can an "apk" app. been installed? It has been installed in a Mobil running Android, but we can not do the same in our iMX508 eval board.
Thanks for your help,
Hello!
I have finally achieve to install my app in two different ways:
1-Copying the app to the sd card:
After positioning myself on the app directory( in the android internal console), I tried:
# pm install app.apk and I received:
Failure [INSTALL_FAILED_INSUFFICIENT_STORAGE]
.
This happened because the app wasn't copied on the correct sd partition.
After changing the location of the app I got another problem:
Failure[INSTALL_PARSE_FAILED_NO_CERTIFICATES]
I have solved this by creating a signed app,copying it and installing it again.(The first app wasn't a signed one).
2- Connecting the device to the pc (LINUX):
I have been able to connect it by following Eduardo's last post steps.
Thank you Eduardo, because testing the apps with the device directly connected to my pc will save me a lot of time.
Thanks also to everybody who has tried to help on solving this issue. If anybody has any question about the topic, I'll be willing to help you.
Regards,
Iker iMX.508.
look this ( FileNotFound*rubg4FIX*SipmC07uz/i.MX_Android_R10.3.1_User_Guide.html )
5.9 How to setup PC (Windows) to support ADB/RNDIS
Before this release, we used HTC's vendor id and product id for all the android gadget functions. It's bad case, so we changed the default android USB gadget functions's VendorID to freescale's 0x15a2, and ProductID to fake ones(after acquiring the offical product id, we will replace them). Due to this change, we must update the PC's USB driver and ADB configuration to enable the android gadget functions:
For Windows PC:
For Linux PC:
# ANDROID 3RD PARTY USB VENDOR ID LIST -- DO NOT EDIT. # USE 'android update adb' TO GENERATE. # 1 USB VENDOR ID PER LINE. 0x15a2 |
SUBSYSTEM=="usb", SYSFS{idVendor}=="15a2", MODE="0666" |
you may want to
i've experience only on i.mx51, but i guess the above should work also on i.mx50.
Hello,
I am working with Raul with the iMX508 device.
First of all, thank you for your quick answer.
I have tried installing it with both Linux and windows O.S. (by default I work on linux), but I as Raul has said, I haven't achieve it.
I have tried installing it via adb, but it doesn't find the device ( it is already on debugger mode).
I have tried installing it copying the app on the SD card directly and then install it through the android internal console. I received a not enough space error.
So I don't what to do, I think that ones I find the way to recognice the device the problem will be solved, but how can I do it? Do I need any extra driver or something like this?
Regards,
Iker.