AOSP 9.0 imx6q sabresd board surfaceflinger crash?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AOSP 9.0 imx6q sabresd board surfaceflinger crash?

1,206 Views
ThanarajS
Contributor III

Please help me on this error.

My Env: imx6q, android 9.0, sabresd, sd card boot

init: starting service 'zygote'...
audit_log_lost: 10 callbacks suppressed
audit: audit_lost=224 audit_rate_limit=5 audit_backlog_limit=64
init: Created socket '/dev/socket/zygote', mode 660, user 0, group 1000
audit: rate limit exceeded
init: starting service 'surfaceflinger'...
init: Failed to bind socket 'pdx/system/vr/display/client': No such file or directory
init: Failed to bind socket 'pdx/system/vr/display/manager': No such file or directory
init: Failed to bind socket 'pdx/system/vr/display/vsync': No such file or directory
DEBUG: *** *** *** *** *** *** *** *** *** *** *** *** *** *** *** ***
DEBUG: Build fingerprint: 'Android/sabresd_6dq/sabresd_6dq:9/2.2.0-ga-rc3/root08231254:userdebug/dev-key'
DEBUG: Revision: '0'
DEBUG: ABI: 'arm'
DEBUG: pid: 286, tid: 286, name: app_process >>> /system/bin/app_process <<<
DEBUG: signal 6 (SIGABRT), code -6 (SI_TKILL), fault addr --------
DEBUG: Abort message: 'Error creating cache dir /data/dalvik-cache/arm : No such file or directory'
DEBUG: r0 00000000 r1 0000011e r2 00000006 r3 ac160768
DEBUG: r4 0000011e r5 0000011e r6 beb7b424 r7 0000010c
DEBUG: r8 beb7caab r9 00000001 r10 00000004 r11 00000004
DEBUG: ip 00000041 sp beb7b410 lr ac0ec105 pc ac0e3e92
DEBUG:
DEBUG: backtrace:
DEBUG: #00 pc 0001ce92 /system/lib/libc.so (abort+62)
DEBUG: #01 pc 00006dd5 /system/lib/liblog.so (__android_log_assert+156)
DEBUG: #02 pc 00001ad7 /system/bin/app_process32 (main+1054)
DEBUG: #03 pc 0008bd89 /system/lib/libc.so (__libc_init+48)
DEBUG: #04 pc 00001677 /system/bin/app_process32 (_start_main+46)
DEBUG: #05 pc 00019a27 /system/bin/linker (__dl__ZNSt3__112__hash_tableINS_17__hash_value_typeIjP6s)
DEBUG: #06 pc 00020b55 [stack:beb5c000]
init: Untracked pid 295 exited with status 0
audit: audit_lost=230 audit_rate_limit=5 audit_backlog_limit=64
audit: rate limit exceeded
print_attach_repeat_log: usb attach timer run
init: starting service 'zygote'...
audit: audit_lost=275 audit_rate_limit=5 audit_backlog_limit=64
init: Created socket '/dev/socket/zygote', mode 660, user 0, group 1000
audit: rate limit exceeded
init: starting service 'surfaceflinger'...
init: Failed to bind socket 'pdx/system/vr/display/client': No such file or directory
init: Failed to bind socket 'pdx/system/vr/display/manager': No such file or directory
init: Failed to bind socket 'pdx/system/vr/display/vsync': No such file or directory
DEBUG: *** *** *** *** *** *** *** *** *** *** *** *** *** *** *** ***
DEBUG: Build fingerprint: 'Android/sabresd_6dq/sabresd_6dq:9/2.2.0-ga-rc3/root08231254:userdebug/dev-key'
DEBUG: Revision: '0'
DEBUG: ABI: 'arm'
DEBUG: pid: 340, tid: 340, name: app_process >>> /system/bin/app_process <<<
DEBUG: signal 6 (SIGABRT), code -6 (SI_TKILL), fault addr --------
DEBUG: Abort message: 'Error creating cache dir /data/dalvik-cache/arm : No such file or directory'
DEBUG: r0 00000000 r1 00000154 r2 00000006 r3 b029d768
DEBUG: r4 00000154 r5 00000154 r6 befde424 r7 0000010c
DEBUG: r8 befdfaab r9 00000001 r10 00000004 r11 00000004
DEBUG: ip 00000041 sp befde410 lr b0229105 pc b0220e92
DEBUG:
DEBUG: backtrace:
DEBUG: #00 pc 0001ce92 /system/lib/libc.so (abort+62)
DEBUG: #01 pc 00006dd5 /system/lib/liblog.so (__android_log_assert+156)
DEBUG: #02 pc 00001ad7 /system/bin/app_process32 (main+1054)
DEBUG: #03 pc 0008bd89 /system/lib/libc.so (__libc_init+48)
DEBUG: #04 pc 00001677 /system/bin/app_process32 (_start_main+46)
DEBUG: #05 pc 00018037 /system/bin/linker (__dl__ZN6soinfoD1Ev+14)
DEBUG: #06 pc 00020a94 [stack:befbf000]
init: Untracked pid 349 exited with status 0
init: Service 'zygote' (pid 340) received signal 6
init: Sending signal 9 to service 'zygote' (pid 340) process group...
libprocessgroup: Successfully killed process cgroup uid 0 pid 340 in 0ms
audit: audit_lost=281 audit_rate_limit=5 audit_backlog_limit=64
audit: rate limit exceeded
audit: audit_lost=335 audit_rate_limit=5 audit_backlog_limit=64
init: Created socket '/dev/socket/zygote', mode 660, user 0, group 1000
audit: rate limit exceeded
init: starting service 'surfaceflinger'...
init: Failed to bind socket 'pdx/system/vr/display/client': No such file or directory
init: Failed to bind socket 'pdx/system/vr/display/manager': No such file or directory
init: Failed to bind socket 'pdx/system/vr/display/vsync': No such file or directory

Thanks

Regards,
Thanaraj Subramani
0 Kudos
Reply
1 Reply

941 Views
igorpadykov
NXP Employee
NXP Employee

Hi Thanaraj

to narrow down issue one can try to reproduce it on Sabre SD reference board with Demo Image

Demo Images – i.MX 6Quad, i.MX 6QualPlus, and i.MX 6DualLite SABRE-SD Boards and Platforms

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply