AGL for imx6q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AGL for imx6q

Jump to solution
3,969 Views
senli
Contributor II

大家好!

       请问飞思卡尔有没有IMX6Q 的AGL(Automotive Grade Linux)BSP包,在哪里可以下载到BSP包。

       另外哪里可以介绍下载下载和编译的文档。

0 Kudos
Reply
1 Solution
3,259 Views
igorpadykov
NXP Employee
NXP Employee

Hi sen

please check

meta-nxp-agl.git - NXP AGL Yocto Project Demo Layer 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
4 Replies
3,260 Views
igorpadykov
NXP Employee
NXP Employee

Hi sen

please check

meta-nxp-agl.git - NXP AGL Yocto Project Demo Layer 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
3,259 Views
senli
Contributor II

你好!

        我参考meta-nxp-agl.git - NXP AGL Yocto Project Demo Layer ,现在已经编译通过,已经跑起来了。

        我的编译命令是

         
DISTRO=nxp-imx-agl-wayland MACHINE=imx6qsabresd source nxp-setup-agl.sh -b bld-agl
bitbake agl-demo-platform

可是,系统起来之后,可以看到开机LOGO,但是LOGO显示后,就没有显示了。没有界面出来,请问还有什么需要配置的地方吗?

0 Kudos
Reply
3,259 Views
305824281
Contributor I

你好,想请教下,你下载用的工具是mfgtools吗,需要更改ucl2.xml文件吗

0 Kudos
Reply
3,259 Views
senli
Contributor II

非常感谢!

另外在请问下有没有类似AGL porting guide之类的文档呢?在哪里可以下载?

0 Kudos
Reply