This in reference to
https://community.nxp.com/t5/i-MX-Processors/Android-A-B-Update-on-i-MX6/m-p/1070152
Is that the imx6 processor can't do an a/b seamless update or that the software support is there only for the imx8? Is it possible to adjust the software for the imx8 in order for it to work for the imx6 if it isn't a processor limitation?
解決済! 解決策の投稿を見る。
Hello nbull,
You can do the port with software, but it won´t work on hardware side because the IPU of the MX6.
Regards
Okay, so pretty much the only solution for a/b seamless updates is using the imx8 and imx-android-10.0.0_2.x.0?
Correct!!