A/B seamless updates on imx6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

A/B seamless updates on imx6

Jump to solution
703 Views
nbull
Contributor II

This in reference to

https://community.nxp.com/t5/i-MX-Processors/Android-A-B-Update-on-i-MX6/m-p/1070152

 

Is that the imx6 processor can't do an a/b seamless update or that the software support is there only for the imx8? Is it possible to adjust the software for the imx8 in order for it to work for the imx6 if it isn't a processor limitation?

Tags (2)
0 Kudos
1 Solution
688 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport
0 Kudos
3 Replies
693 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello nbull,

You can do the port with software, but it won´t work on hardware side because the IPU of the MX6.

 

Regards

 

0 Kudos
691 Views
nbull
Contributor II

Okay, so pretty much the only solution for a/b seamless updates is using the imx8 and imx-android-10.0.0_2.x.0?

0 Kudos
689 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Correct!!

 

0 Kudos