8MMINILPD4-EVK up-to-date version of the schematic

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

8MMINILPD4-EVK up-to-date version of the schematic

ソリューションへジャンプ
1,105件の閲覧回数
broz
Contributor I

Hi,

I have an i.MX8 M Mini LPDDR4 EVK (8MMINILPD4-EVK), the hardware is in version C3 (SCH-31399 REV C3), but the documentation (mainly schematic) from the official NXP product page is only in version C2. Are there any changes in the schematic between versions? Does NXP provide an up-to-date version of the documentation?

Thanks,

Jan

ラベル(1)
タグ(1)
0 件の賞賛
1 解決策
1,045件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Jan,

The schematics are often updated on the web but sometimes they may lag from the versions being shipped.

The changes between C2 and C3 are:

  1. Update U8 Part Number BD71847MWV-E2 to BD71847AMWV-E2;
  2. Populate R106, as external PU is necessary for Boundary Scan Mode, also update the note;
  3. Add note for Boundary Scan mode: BOOT_MODE0, BOOT_MODE1, JTAG_MOD and TEST_MODE must be pulled to "1101" for i.MX8M Mini to enter Boundary Scan mode;

If you are interested in the updated schematic files, I would need to ask you to please open a support ticket on the link below. Hopefully they will be updated on the webpage soon.

https://www.nxp.com/support/support:SUPPORTHOME

I hope this helps!

Regards,

元の投稿で解決策を見る

0 件の賞賛
1 返信
1,046件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Jan,

The schematics are often updated on the web but sometimes they may lag from the versions being shipped.

The changes between C2 and C3 are:

  1. Update U8 Part Number BD71847MWV-E2 to BD71847AMWV-E2;
  2. Populate R106, as external PU is necessary for Boundary Scan Mode, also update the note;
  3. Add note for Boundary Scan mode: BOOT_MODE0, BOOT_MODE1, JTAG_MOD and TEST_MODE must be pulled to "1101" for i.MX8M Mini to enter Boundary Scan mode;

If you are interested in the updated schematic files, I would need to ask you to please open a support ticket on the link below. Hopefully they will be updated on the webpage soon.

https://www.nxp.com/support/support:SUPPORTHOME

I hope this helps!

Regards,

0 件の賞賛