5.4.3 Linux version run jh_mmcboot issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

5.4.3 Linux version run jh_mmcboot issue

770件の閲覧回数
hongxingyu1982
Contributor III

Now I used 5.4.3 Linux + imx8mq board, and I would like to boot the jailhouse root cell, when I run jh_mmcboot in u-boot, it hang at rootfs with sd card as blew:

pastedImage_1.png

It seems the sd card issue, but I have modify any code. 

Could anyone alse face this issue ?and How can fix it ?

BR

0 件の賞賛
3 返答(返信)

700件の閲覧回数
hongxingyu1982
Contributor III

And the 4.4 kernel version is no this issue.

0 件の賞賛

700件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Hongxing,

In this release, the virtualization (Xen, Jailhouse) feature is not verfied or tested. Recommend you to use other version BSP.

Have a nice day

Best Regards

Rita

0 件の賞賛

700件の閲覧回数
hongxingyu1982
Contributor III

Is there anyone face the same issue ?

0 件の賞賛