2 channel 720P@30 video capture in single SoC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2 channel 720P@30 video capture in single SoC

418 Views
shabbirlimdiwal
Contributor I

Hi,

Can i.mx6 Quad capture 2 video input of 720P@30 each simultaneously ? Can it be done with CSI ? Can it be done with parallel ?

Regards,

Shabbir

0 Kudos
1 Reply

312 Views
igorpadykov
NXP Employee
NXP Employee

Hi Shabbir

yes it can. Performance is given in IMX6DQRM 37.1.2.1.1 Camera Ports:

for parallel interface, the maximum speed of the interface is 240Mhz.

for MIPI for 4 data lanes configuration : 400MByte/sec

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos