12.01 iMX53 Linaro Release Candidate
We've got a great RC for people to look at:
https://android-build.linaro.org/builds/~linaro-android/staging-imx53-12.01-release/#build=6
Here's the test results:
We're working to get an accelerated version on iMX53 going, before moving onto iMX6.
Always happy to get feedback!
I dont think the linaro uImage is fully compatible with my tablet but I will give it a go at a later stage if the system image work. Is the current uImage able to boot mx51/mx53 now? Previously, it has to compile specifically for each platform.
I think so. Give it a go. Its easy to replace the kernel. Just follow the instructions listed on the build site and then
Mount the first partition:
$mkdir mnt
$sudo mount /dev/sdc1 mnt
If you do a
$ls mnt
You’ll see a uImage among the files. Copy the uImage that was built over.
$sudo cp arch/arm/boot/uImage mnt
Unmount and sync:
$sudo umount mnt
$sync
(seen on this post http://www.linaro.org/linaro-blog/2011/09/15/switching-out-a-pre-built-android-images-kernel/)
More documentation can be found here:
thanks, Zach.
Thats was my only intention. To reuse the linaro android ics source only and not the boot and kernel image. I was just wondering if the libraries for mx53 is compatible with mx51 especially when the hardware acceleration is available.
Killerkink, the way we do our builds is fairly extensible. You could probably look at how we did the iMX53 and make a few changes to our build to bring in iMX51. It may be as simple as just using our build directly (including the linaro-android-media-create step) the just replacing the kernel with your iMX51 kernel.
No. What do you have running on the iMX51?