12.01 iMX53 Linaro Release Candidate -blog archive

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

12.01 iMX53 Linaro Release Candidate -blog archive

1,558 Views
ZachPfeffer
Contributor II

12.01 iMX53 Linaro Release Candidate 

We've got a great RC for people to look at:

https://android-build.linaro.org/builds/~linaro-android/staging-imx53-12.01-release/#build=6

Here's the test results:

https://docs.google.com/a/linaro.org/spreadsheet/ccc?key=0AkxwyUNxNaAadHlNN1hZZERMbThtaTBlSkZwVDRYdG...

We're working to get an accelerated version on iMX53 going, before moving onto iMX6.

Always happy to get feedback!

Tags (1)
0 Kudos
Reply
7 Replies

1,387 Views
Hock
Contributor I

I dont think the linaro uImage is fully compatible with my tablet but I will give it a go at a later stage if the system image work. Is the current uImage able to boot mx51/mx53 now? Previously, it has to compile specifically for each platform.

0 Kudos
Reply

1,387 Views
ZachPfeffer
Contributor II

I think so. Give it a go. Its easy to replace the kernel. Just follow the instructions listed on the build site and then 

Update the Kernel

Mount the first partition:

$mkdir mnt
$sudo mount /dev/sdc1 mnt

If you do a

$ls mnt

You’ll see a uImage among the files. Copy the uImage that was built over.

$sudo cp arch/arm/boot/uImage mnt

Unmount and sync:

$sudo umount mnt
$sync

(seen on this post http://www.linaro.org/linaro-blog/2011/09/15/switching-out-a-pre-built-android-images-kernel/)

More documentation can be found here: 

https://wiki.linaro.org/Platform/Android

0 Kudos
Reply

1,387 Views
Hock
Contributor I

thanks, Zach.

Thats was my only intention. To reuse the linaro android ics source only and not the boot and kernel image. I was just wondering if the libraries for mx53 is compatible with mx51 especially when the hardware acceleration is available.

0 Kudos
Reply

1,387 Views
ZachPfeffer
Contributor II

Killerkink, the way we do our builds is fairly extensible. You could probably look at how we did the iMX53 and make a few changes to our build to bring in iMX51. It may be as simple as just using our build directly (including the linaro-android-media-create step) the just replacing the kernel with your iMX51 kernel.

0 Kudos
Reply

1,387 Views
Hock
Contributor I

i have the modified source for freescale r10.3.1 running on kernel v2.3.35. I was thinking if its possible to use some of the library in linaro android for mx53 and port it to CM9 running on imx515.

0 Kudos
Reply

1,387 Views
ZachPfeffer
Contributor II

No. What do you have running on the iMX51?

0 Kudos
Reply

1,387 Views
Hock
Contributor I

will it work on mx51?

0 Kudos
Reply