请问哪里可以找到android_jb4.2.2_1.1.0-ga_source.tar.gz文件包?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

请问哪里可以找到android_jb4.2.2_1.1.0-ga_source.tar.gz文件包?

2,029 Views
daqiang
Contributor I

网站上只能看到4.3和4.4的部分

http://www.freescale.com/zh-Hans/webapp/sps/site/prod_summary.jsp?code=IMX6_SW

还请帮忙提供链接

谢谢!

Labels (2)
0 Kudos
Reply
7 Replies

1,606 Views
saurabh206
Senior Contributor III
0 Kudos
Reply

1,606 Views
daqiang
Contributor I

Hi Saurabh:

     Do you have 4.2.2.1.1.0 version? The link you provide to me is version 4.2.2.1.0.0。

Thanks!

0 Kudos
Reply

1,606 Views
saurabh206
Senior Contributor III

No I have 4.2.2.1.0.0

0 Kudos
Reply

1,606 Views
daqiang
Contributor I

Freescale的文档中有提到android_jb4.2.2_1.1.0-ga_source.tar.gz这个包,我们也希望用这个版本,

那要到哪里才能找得到呢?

谢谢!

0 Kudos
Reply

1,606 Views
SergioSolis
NXP Employee
NXP Employee

Hello Guo,

Android 4.2.2.1.1 is no longer maintained by us but you can download newer versions of android from the following link:

i.MX6Q|i.MX 6Quad Processors|Quad Core|Freescale


Have a great day,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,606 Views
daqiang
Contributor I

明白了。

另外一个问题,目前网站上最新的是4.4,请问这个版本目前是什么状况?到哪个阶段了?

如果我们使用4.4的版本,还有哪些已知的问题吗?

多谢!

0 Kudos
Reply

1,606 Views
SergioSolis
NXP Employee
NXP Employee

The latest BSP release is 4.4.3.2 and it was release in February, so it is supported right now.

The next release will be Lollipop (v5.0) though there is still no release date confirmed.

0 Kudos
Reply