我的imax51开发板,自带的sd卡丢失了。如何恢复自带的sd卡内的Ubuntu系统?谢谢

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

我的imax51开发板,自带的sd卡丢失了。如何恢复自带的sd卡内的Ubuntu系统?谢谢

734 Views
chengzhiyan
Contributor I

我的imax51开发板,自带的sd卡丢失了。如何恢复自带的sd卡内的Ubuntu系统?谢谢

0 Kudos
Reply
3 Replies

586 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi chengzhi yan,

Which board are you using , is it the board i.MX51 Evaluation Kit you buy from NXP ? If yes, you can use the mfgtool in our website to write the images to the SD on your board. The Root File System for the Ubuntu Demo image you can download from our website. The link is :

i.MX51 Evaluation Kit|NXP . You can see it under the

Root File System for the Ubuntu Demo Image. ER 2010.11 for i.MX51. Engineering Release (REV ER2010.11)

  Root File System for the Ubuntu Demo Image. ER 2010.11 for i.MX51. Engineering Release.

Hope this can help you.

Have a nice day.

Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

586 Views
chengzhiyan
Contributor I

It is ok,thank you!

0 Kudos
Reply

586 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi chengzhi yan,

:smileyhappy:I am very glad it can help you. If this post answers your question, please click the Correct Answer button. Thank you!

Have a nice day

Best Regards

Dan

0 Kudos
Reply