如何编译用于MFGTools工具的uboot和kernel镜像

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

如何编译用于MFGTools工具的uboot和kernel镜像

1,988 Views
1182614726
Contributor III

大家好,

      

            我们参考官方imx6dl EVB做了一块自己的开发板,因DDR大小及串口配置与官方EVB板配置不一致,导致目前无法升级软件。分析ucl2.xml文件,应该是MFGTools工具用的uboot和kernel镜像不对,请问要如何配置生成MFGTools使用的镜像呢?非常感谢

Labels (1)
0 Kudos
Reply
2 Replies

1,685 Views
joanxie
NXP TechSupport
NXP TechSupport

you can refer to the "Manufacturing Tool V2 Linux or Android Firmware Development Guide V2.docx" in the mfgtool folder, I don't know what bsp version you use, I attach the 4.9.11 for reference, it should be the same steps, you also can find it under mfgtools>Document>v2

0 Kudos
Reply

1,685 Views
1182614726
Contributor III

你好,

      我使用的是yocto编译的L4.1.15-2.1.0 BSP包。

      我目前使用bitbake linux-mfgtool bitbake u-boot-mfgtool bitbake fsl-image-mfgtool-initramfs 分别重新编译了uboot,kernel,ramdisk.gz,现在烧写的时候,uboot可以跑起来,加载完kernel和ramdisk.gz和devicetree后,停在了starting kernel...,复位后按任何键进入不了uboot命令行界面,暂不确定是什么原因,请帮忙鼎力支持。

0 Kudos
Reply