你好:
我们现在相同的主板分别搭载了imx6dl 和imx6d cpu
在关机充电时,会进入关机充电态,这时候会显示电池图片。
现在imx6d cpu 在关机充电态时,是会显示电池图片的。
但是imx6dl cpu 在进入关机充电态后,却不能显示图片,屏无任何图片显示。但是在uboot、kernel、android下,dl cpu 显示都是正常的。
以下是imx6dl cpu在充电态下的一些日志。
charger:
charger: ************* END LAST KMSG *************
charger:
charger: --------------- STARTING CHARGER MODE ---------------
failed to read font: res=-1
can't open /dev/tty0: No such file or directory
framebuffer: fd 4 (720 x 1280)
以下的则是imx6q的一些日志
No errors detected
charger:
charger: ************* END LAST KMSG *************
charger:
charger: --------------- STARTING CHARGER MODE ---------------
type=1400 audit(86454.500:4): avc: denied { entrypoint } for pid=2279 comm="init" path="/sbin/healthd" dev=rootfs ino=1476 scontext=u:r:healthd:s0 tcontext=u:object_r:rootfs:s0 tclass=file
healthd: wakealarm_init: timerfd_create failed
healthd: BatteryTemperaturePath not found
healthd: BatteryTechnologyPath not found
: No such file or directory
init: cannot expand '${sys.sysctl.extra_free_kbytes}' while writing to '/proc/sys/vm/extra_free_kbytes'
init: property 'persist.sys.usb.config' doesn't exist while expanding '${persist.sys.usb.config}'
init: cannot expand '${persist.sys.usb.config}' while assigning to 'sys.usb.config'
framebuffer: fd 4 (720 x 1280)
which bsp are you using?