usb2作为host,其ID已经直接接地,VBUS悬空,设备采用外部供电方式。设备树中加载了usb2的驱动
usbotg2: usb@02184200 {
compatible = "fsl,imx6ul-usb", "fsl,imx27-usb";
reg = <0x02184200 0x200>;
interrupts = <GIC_SPI 42 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&clks IMX6UL_CLK_USBOH3>;
fsl,usbphy = <&usbphy2>;
fsl,usbmisc = <&usbmisc 1>;
ahb-burst-config = <0x0>;
tx-burst-size-dword = <0x10>;
rx-burst-size-dword = <0x10>;
status = "disabled";
};
&usbotg2 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_usbotg2>;
dr_mode = "host";
disable-over-current;
status = "okay";
};
现在的问题是,系统启动后,在/sys/bus/usb/devices 下只能看到
1-0:1.0@ usb1@
如果给外部设备开机,系统一直在提示下面的信息:
usb 1-1: new high-speed USB device number 119 using ci_hdrc
但是无法识别出设备来,如果usb1接上外部设备了,usb2上就识别出来了,这是怎么回事
Hello JiYong,
USB VBUS couldn't be floated, it should be supplied 5V power. try it , please!
Have a great day,
TIC weidong sun
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
非常感谢您的回复,我测试后发现确实VBUS必须接入确定的高电平。