使用KSZ9031 IC,Ethernet 无法使用1000M Lan

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

使用KSZ9031 IC,Ethernet 无法使用1000M Lan

3,180 Views
daqiang
Contributor I

我们使用的是KSZ9031方案,如果设置成10M/100M都没问题,但如果设置成1000M,则无法连接。

路由器是支持1000M的。

Labels (2)
0 Kudos
Reply
3 Replies

2,858 Views
chenw
Contributor II

请问是怎么修复的呢,千兆不可用的情况

0 Kudos
Reply

2,858 Views
igorpadykov
NXP Employee
NXP Employee

Translated by Google:

Use KSZ9031 IC, Ethernet can not use the 1000M Lan
We are using KSZ9031 scenario, if set to 10M / 100M no problem, but if set to 1000M, you can not connect.
Router supports the 1000M.

-------------------------------------------------

Hi Guo

suggest to check Table 62. RGMII Signal Switching Specifications IMX6DQCEC

and configure KSZ9031 registers if necessary, like

MMD Address 2h  Register 5h - RGMII RX Data Pad Skew

MMD Address 2h  Register 6h - RGMII TX Data Pad Skew

MMD Address 2h  Register 8h - RGMII Clock Pad Skew

Note, for i.MX6 ENET there is no control on-chip to adjust the delay between

these signals. A delay would need to be implemented at the board level.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,858 Views
daqiang
Contributor I

Hi :

It works now,thanks!

But there is another problem. As we know,IMX6DL ethernet's max speed is 400M,but we can only reach 200M,is there other registers we should adjust?

Thank you!

Regards!

Leo GUo

0 Kudos
Reply