i.MX6DQ Register Programming Aids

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6DQ Register Programming Aids

i.MX6DQ Register Programming Aids

Important: If you have any questions or would like to report any issues with the DDR tools or supporting documents please create a support ticket in the i.MX community. Please note that any private messages or direct emails are not monitored and will not receive a response.

 

These are the detailed programming aids for the registers associated with MMDC DDR3 and LPDDR2 initialization for the MX6DQ SoC. The last sheet formats the register settings for use with ARM RealView ICE. It can also be used with the windows executable for the DDR Stress Test. This programming aid was used for internal NXP boards.

 

Labels (2)
Attachments
0% helpful (0/1)
Version history
Last update:
‎03-27-2024 03:44 PM
Updated by: