Wifi cannot work on Android layer with i.MX6 SABRE-SD board kernel 3.0.35 kitkat4.4.2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Wifi cannot work on Android layer with i.MX6 SABRE-SD board kernel 3.0.35 kitkat4.4.2

Wifi cannot work on Android layer with i.MX6 SABRE-SD board kernel 3.0.35 kitkat4.4.2

For detailed view, please check out the attached file.

Tags (2)
Attachments
Comments

Hi All,

I am also facing the same problem, Please help me to get out of this problem.

Platform : IMX6SL

Bluedroid on Android kitkat 4.4.3.

  Can you please help me I am struck at this point not able to move forward.

D/BluetoothAdapterState( 704): CURRENT_STATE=PENDING, MESSAGE = ENABLE_TIMEOUT, isTurningOn=true, isTurningOff=false

E/BluetoothAdapterState( 704): Error enabling Bluetooth

D/BluetoothAdapterProperties( 704): Setting state to 10

I/BluetoothAdapterState( 704): Bluetooth adapter state changed: 11-> 10

D/BluetoothAdapterService( 704): Broadcasting updateAdapterState() to 1 receivers.

Hi all,

  I am glad to inform you that the above issue which I have posted earlier got resolved, but I have another 2 issues one while data transfer, the other while enabling via GUI.

   1) After enabling bluetooth, while transferring file from third party mobile to IMX_6SL board, file is getting transferred(TX), but vice versa (RX) is not happening, it is giving the error message :

   File not Received

   File : sample.jpg

   Reason : Storage issue

  2) And presently I am inserting my driver via GUI, I am getting an error message while enabling bluetooth via GUI   ie Operation not permitted while loading .ko (driver)Please suggest me what to do?? whether I need to install my driver at boot by adding in init.rc?? if I do it always on boot bt will be in ON State only??  OR Do i need to build my driver along with android source code???

Please suggest me how to proceed further???

Thanks and Regards,

Mutyala Rao.

Hi all,

   I am able to resolve the above two issues like this.

1. Installed the apk.file using ADB (Android Debugger) by following this link:

     https://androidonlinux.wordpress.com/2013/05/12/setting-up-adb-on-linux/

2. I have inserted the modules on boot. by placing the path of the modules in init.freescale.rc located in the path myandroid/out/target/product/evk_6sl/root/

Hi Mutyalarao,

I am facing the same issue with you. Could you tell me how did you solve this issue when turn on wifi?

Very appreciate.

root@sabresd_6dq:/ # D/WifiService( 2727): setWifiEnabled: true pid=3073, uid=1000

W/WifiHW  ( 2727):

W/WifiHW  ( 2727): ---------------SN=--------->>>>>>>wifi_load

_driver

E/WifiHW  ( 2727): +++++type=1400 audit(86590.640:5): avc:  denied  { module_request } for  pid=2681 comm="netd" kmod="netdev-wlan0" scontext=u:r:netd:s0 tcontext=u:r:kernel:s0 tclass=system

+ wifi_load_driver

type=1400 audit(86590.660:6): avc:  denied  { sys_module } for  pid=2681 comm="netd" capability=16  scontext=u:r:netd:s0 tcontext=u:r:netd:s0 tclass=capability

type=1400 audit(86590.680:7): avc:  denied  { module_request } for  pid=2681 comm="netd" kmod="netdev-wlan0" scontext=u:r:netd:s0 tcontext=u:r:kernel:s0 tclass=system

type=1400 audit(86590.700:8): avc:  denied  { sys_module } for  pid=2681 comm="netd" capability=16  scontext=u:r:netd:s0 tcontext=u:r:netd:s0 tclass=capability

type=1400 audit(86590.710:9): avc:  denied  { module_request } for  pid=2681 comm="netd" kmod="netdev-wlan0" scontext=u:r:netd:s0 tcontext=u:r:kernel:s0 tclass=system

type=1400 audit(86590.720:10): avc:  denied  { sys_module } for  pid=2681 comm="netd" capability=16  scontext=u:r:netd:s0 tcontext=u:r:netd:s0 tclass=capability

type=1400 audit(86590.740:11): avc:  denied  { module_request } for  pid=2681 comm="netd" kmod="netdev-wlan0" scontext=u:r:netd:s0 tcontext=u:r:kernel:s0 tclass=system

type=1400 audit(86590.760:12): avc:  denied  { sys_module } for  pid=2681 comm="netd" capability=16  scontext=u:r:netd:s0 tcontext=u:r:netd:s0 tclass=capability

type=1400 audit(86590.780:13): avc:  denied  { module_request } for  pid=2681 comm="netd" kmod="netdev-wlan0" scontext=u:r:netd:s0 tcontext=u:r:kernel:s0 tclass=system

Thanks,

Wayne

No ratings
Version history
Last update:
‎06-04-2015 07:28 AM
Updated by: