Using Manufacturing Tool for iMX28 in Win7 64-bit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using Manufacturing Tool for iMX28 in Win7 64-bit

Using Manufacturing Tool for iMX28 in Win7 64-bit

A new release of the manufacturing tool is was recently made available, "imx-3.10.53_1.1.0_ga-mfg-tools".

It can be found in the software download sections for the iMX6 family.

However, it can be used to program an iMX28 in a Win7 64-bit host by adding a few files.

The steps to do so are listed below and can be checked against the script in ucl2.xml.

  1.   Download the attached "28.vbs" file and place it into where the manufacturing tool was installed, typically in  <install_dir>\mfgtools\
  2.   Replace <install_dir>\mfgtools\Profiles\Linux\OS Firmware\ucl2.xml with the attached ucl2.xml. 
  3.   Copy the attached files "updater_ivt.sb" and "fdisk-u.input" into <install_dir>\mfgtools\Profiles\Linux\OS Firmware\firmware
  4. Copy your iMX28 image file into <install_dir>\mfgtools\Profiles\Linux\OS Firmware\files.  The file should be renamed to "linux.sb" to conform with the ucl2.xml script.
  5. Copy your "rootfs.tar.bz2" file into <install_dir>\mfgtools\Profiles\Linux\OS Firmware\files

To launch the manufacturing tool, double click on "28.vbs".

Issue:

After MfgTool has finished and the progress bars have turned green, clock on the Stop button or the program will start another cycle.

ラベル(1)
添付
コメント

Please add the link to the download menue of mfg-tool. There is no chance to find the software at the freescale download center!!.

Thank you

Siegfried

It supports a wide variety of file formats and a wide range of camcorders and cameras including Low resolution camcorder (Raw and AVI DV editing), Mpeg2, mpeg4 and h264 AVCHD (small cameras and camcorders), High resolution camcorder files, including HDV and AVCHD camcorders, Professional camcorders, including XDCAM-HD™ streams, IMX™ (D10) streams, DVCAM (D10) , DVCAM, DVCPRO™, DVCPRO50™ streams and DNxHD™ streams.

see: https://luckypatcher.pro/

https://kodi.software/

https://plex.software/

SKF @ptitude Analyst DMx Manager Software Suite will install without any problems on a Windows 7, 64-bit operating system. 

評価なし
バージョン履歴
最終更新日:
‎02-13-2015 01:21 PM
更新者: